Scheduled Action Objects

These Action Objects (AO) are user defined calculations scheduled to execute at defined intervals. The Action Object Manager provides valuable information about these processes.

Header

Description

Name

The name given to the AO, saved in the application creating the blueprint. The default name is the name of the file and the AO will be deployed with this name. If a name clash occurs, names will automatically be made unique.

Status

  • Scheduled: The Action Object has been scheduled to execute at a time in the future.

  • Executing:The Action Object is executing.

  • Error: The Action Object is not executing. Refer to the Event Log to see possible causes of the error. To restart the Action Object, either remove the Action Object from the server, and re-add it, or restart the Action Object services.

Next execute

The time when the next execution of the scheduled blueprint will begin.

Last start

The start time of the last executed AO.

Last end

The end time of the last executed AO.

Period

The duration of the execution of the AO.

Executes

The number of AO executions that have been completed.

Average

The average execution time of the AO.

Total time

The amount of time lapsed since the first execution of the scheduled AO.


Related topics:

 

CSense 8.5- Last updated: July 10,2025